FactoryTalk AssetCentre Web Client Interface

Assets shows by default when FactoryTalk AssetCentre web client opens.
IMPORTANT:
Before using FactoryTalk AssetCentre web client, configure security settings for assets in the FactoryTalk AssetCentre desktop client to ensure that users' access and rights are limited according to the customer's application needs.
For more information, see Change security settings for an asset in the
FactoryTalk AssetCentre Desktop Client Help
.
FactoryTalk AssetCentre Web Client
Interface Element
Description
callout1
Signed-in User
Shows the user account that signs in to FactoryTalk AssetCentre web client.
CallOut2
Toolbar
The toolbar includes:
  • Assets
  • Logs
  • Schedules
  • Lifecycle Information
  • Security Compliance
  • Searches
  • Tools
CallOut3
Asset
Contains the asset tree and the archive workspace. The assets tree represents the assets deployment structure in your plant, and the archive workspace is the same as the
Archive
tab in the FactoryTalk AssetCentre desktop client.
CallOut4
Help
Opens the Help.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal