State Name
The tag value is shown as State name on the training page. If there is a change in the tag
value , a separate tab is created, using the tag value for the State name. For example, the
value for the tag selected during controller configuration is 'State A', then the
state name is 'State A'.
State Name

Following is an example image where the component has multiple states.
Multiple States

In the above example, 'State A' is called the
Current State
. It can also be
referred as active state. The name of the Current State is denoted with bold text, blue bottom
border and a green dot indicating active. The active state is always available on the left
side. The states which are inactive are grouped together and a pagination control is available
to select the required state. When a particular state is selected, a blue underline appears giving focus on which inactive
state the user is currently in focus. The system automatically sorts inactive states by
creation timestamp, ensuring the most recently created state appear first across the
sequence.
If multiple state definition tags are selected on the
State Definition
page during controller configuration, the state name will be displayed as "<tag1-value><tag2-value>".Provide Feedback