Monitoring Status
On the Training page of a component, the user can view the following status in the Monitoring Status section:
- Source Controller Connection Status: When the Controller is configured, the status is displayed as green andSource controller connected. For the default state, it is displayed asSource controller not configured.
- Controller path: The path of the controller is displayed. For the default state, it is displayed as '--'.
- Monitoring Tag status: When the monitoring tag is selected, the status is displayed as green andMonitoring tag on. For the default state, it is displayed as grey, andNo monitoring tag selected.
- Current Frequency: The current frequency at which the component operates is displayed.
- Current State: Name of the active state is displayed here. For the default state, it is displayed as '--'.
- Output Controller Connection Status: When the output controller is configured, the status is displayed as green andOutput controller Connected. For the default state, it is displayed asOutput controller not configured.
Monitoring Status

If only one tag is selected on the State Definition page, and if the tag is invalid, training
and monitoring will be stopped. A message is displayed in red, as shown in the following
image, and the current state will be shown as
--
.If multiple tags are selected and all the tags are invalid, training and monitoring will be stopped.
Monitoring Status for Invalid Tags

Provide Feedback