Bearing Monitoring

The bearing dimensions are used by the FactoryTalk Analytics GuardianAI algorithm to provide first principle failure mode recommendations. The failure modes included in the bearing dimensions are ball bearing fault, inner race bearing fault, outer race bearing fault, and bearing cage fault. If the values are left empty, FactoryTalk Analytics GuardianAI will not include those fault modes in the first principle recommendations when a deviation from normal is detected.
  • Inner Race Multiplier:
    [decimal number input] - BPFI (Ball Pass Frequency Inner) or inner race failing frequency. Corresponds physically to the number of balls or rollers that pass through a given point of the inner track each time the shaft makes a complete turn.
  • Outer Race Multiplier:
    [decimal number input] - BPFO (Ball Pass Frequency Outer) or outer race failing frequency. Corresponds physically to the number of balls or rollers that pass through a given point of the outer race each time the shaft makes a complete turn.
  • Rolling Element Multiplier
    : [decimal number input] - BSF (Ball Spin Frequency) or rolling element failing frequency. Corresponds physically to the number of turns that a bearing ball or roller makes each time the shaft makes a complete turn.
  • Cage Multiplier
    : [decimal number input] - FTF (Fundamental Train Frequency) or Cage failing frequency. Corresponds physically to the number of turns that make the bearing cage each time the shaft makes a complete turn.
Bearing Overview
NOTE: A database containing information on over 7,000 bearings from common manufacturers and models is available. For assistance, please contact your Rockwell Automation Technology Consultant.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal