Components on the Flash Devices tab
The following table explains each item on the
Flash Devices
tab when ControlFLASH Plus
can access the Product Compatibility and Download Center.Item | Description |
|---|---|
Browsing from path | Shows the starting browse path as configured in the Network Browser. By default, it shows the highest node of the network topology. For subsequent uses, it shows the last selected path in the previous session. |
Filter by device | Filters one or more device types in a flashing session. The device list is filtered immediately as the text included in the device name is entered. The number of selected devices, filtered devices, and all devices shows on the left of the Filter by device box.An orange highlight indicates that a filter is active. |
Selection accelerator | Accelerates the device selection in the list with the following options:
Make sure that the Flash To revisions are set before using the selection accelerator. |
Device | The Device column shows the network topology as returned by the browsing path. Network and chassis node names are shown in lighter gray to maintain the hierarchy.An orange highlight on the left border of this column indicates that a filter is active. |
Lifecycle Status | Shows the device's lifecycle status found in the Product Compatibility and Download Center.
Tip : When the Internet connectivity to the Product Compatibility and Download Center is not available, the lifecycle status is not shown.You can visit https://www.rockwellautomation.com/global/support/product-compatibility-migration/lifecycle-status/overview.page
for more information. |
Address | The Address column shows the address of the device, for example, the slot number for devices in backplanes.Tip : Hovering over the address of a device will display a tooltip showing the complete address path to the device. |
In Device | The In Device column shows each device's current firmware revision.When ControlFLASH Plus can access the Product Compatibility and Download Center, the firmware revision lifecycle states are shown. |
Flash To | The Flash To column shows the revisions available on the computer and from the Product Compatibility and Download Center.When ControlFLASH Plus is disconnected to the Product Compatibility and Download Center, the firmware revisions that you select from the Product Compatibility and Download Center will be remained but unavailable. Once connected to the Internet, the firmware revision becomes available.When ControlFLASH Plus can access the Product Compatibility and Download Center, the latest firmware revisions from the Product Compatibility and Download Center are set as default and the following icons are visible.
|
When ControlFLASH Plus can access the Product Compatibility and Download Center, the firmware revision lifecycle states are shown.
Visit Product Compatibility and Download Center for more information. | |
ControlFLASH Plus check In Device firmware revisions and Flash To firmware revisions compatibility and provide compatibility information based on data from the Product Compatibility and Download Center. When compatibility issues appear, the following icons are shown.
Click or to open the Compatibility dialog box. | |
Latest from Download Center | Accelerates the revision selection in the Flash To column with the following options:
|
Status | Shows the status of the flashing workflow. |
Create Favorite List | Creates a favorite list based on the current device and revision selections. This is turned on only when at least one device is selected. |
Compatibility issues | Shows the total number of compatibility issues that occurred during the compatibility check process. Click to open the Compatibility dialog box. |
![]() | Shows the total number of errors that occurred during download. In this example, five errors occurred during download. Tip : The errors will not impact the flashing of devices whose firmware revisions are already downloaded. |
Next | Starts the flashing workflow. This is turned on only when at least one device is selected. |
Provide Feedback










to open the