Compatibility dialog box
How do I open the Compatibility dialog box?
- On theFlash Devicestab, click
,
, or Compatibility Issues.
ControlFLASH Plus
provides compatibility information after selecting firmware revisions to flash. Incompatible firmware revisions may cause some issues to the devices. Use the Compatibility
dialog box to:- Check compatibility information.
- Select compatible firmware revisions to flash.
- Ignore incompatible devices as needed.
Provide Feedback