Components
The following table explains the items in the
Compatibility
dialog box and their meanings.Item | Description |
|---|---|
Lock Revision | This column shows the current device's locked or unlocked status. Hover over the blank cell and click to lock the current device revision. The unlocked devices' compatible choices will be updated to ensure the compatibility with the locked device revision.Lock one or multiple devices as needed. Unlock the locked devices if there are no compatible firmware revisions. |
Current Choices | This column shows the following subcolumns:
|
Compatible Choices | This column shows suggested compatible firmware revisions.
Indications appear if there are locked devices and no compatible firmware revisions. |
Ignore incompatible firmware revisions | This column shows the delete icons. Click Flash Devices tab. |
Provide Feedback
to lock the current device revision. The unlocked devices' compatible choices will be updated to ensure the compatibility with the locked device revision.