Pulse Width Modulation view

The
Pulse Width Modulation
view provides precise, onboard control of an output's pulse train with no program variability. To configure a PWM signal, define two real-time values for the pulse train.
  • Cycle time - The pulse cycle duration in seconds. Valid times range from 1 millisecond to 1 hour.
  • On time - The pulse width, or time that a pulse is active within a cycle. Valid time range from 200 microseconds to 1 hours. On time can also be defined as a percentage of the cycle time.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal