Points view (output)

Use the
Points
view to configure 1756-OB16IEF and 1756-OB16IEFS digital devices:
  • Select a value to determine the behavior of each output when the controller transitions to Program mode.
  • Select a value to determine the behavior of each output when the connection from the controller to the output device is broken (that is, communication to the output device is established and then communication fails).
  • Reset electronic fuse.
  • Sets the result of a communications failure in Program mode.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal