Publishing Libraries
Publishing libraries makes these available from the repository for use in other projects. Publish a library after checking in the library. Publish libraries that are created in projects.
When publishing a library, enter this information:
Name | The name of the library |
Version | The version number of the library. Enter numerical values. |
Comment | Free-format text |
To publish a library
- From theApplication View, select the library to publish.
- From theFilemenu, point toVersion Control, and then clickCheck In.
- In theCheck Indialog box, select whether to keep the library checked out, and then clickOK.
- Right-click the library, and then clickPublish Library.
- In thePublishdialog box, enter a name, version, and comment for the library, and then clickPublish.TIP: Use only numerical values for the library version. Using a non-numerical value causes theAdd Published Librarydialog box to display a blank library version.A copy of the library appears in the repository.
Provide Feedback