GSTATUS Statement in SFC Action
Returns the current status of a Sequential Function Chart (SFC) program.
GSTATUS is not part of the IEC 61131-3 standard.
GSTATUS Statement | |
|---|---|
Name: | GSTATUS |
Syntax: | < var > := GSTATUS ( <child_name > ); where child_name represents the name of the SFC child POU |
Operands: | the specified SFC program must be a child of the one in which the statement is written |
Return value: | 0 = Program is inactive (killed) 1 = Program is active (started) 2 = Program is frozen |
To insert a GSTATUS statement
- In the language container, typeGSTATUS.
Provide Feedback