GFREEZE Statement in SFC Action
Freezes a child Sequential Function Chart (SFC) (program or function block); suspends its execution. The suspended SFC program organization unit (POU) can then be restarted using the GRST statement.
Children of the child program are automatically frozen along with the specified program.
GFREEZE is not part of the IEC 61131-3 standard.
GFREEZE Statement | |
|---|---|
Name: | GFREEZE |
Syntax | GFREEZE ( <child_name> ); where child_name represents the name of the SFC child POU |
Operands | the specified SFC program must be a child of the one in which the statement is written |
Return value: | (none) |
To insert a GFREEZE statement
- In the language container, typeGFREEZE.
Provide Feedback