Transition Clearing Forcing

Force the clearing of a transition while in simulation whether all previous steps are active or not. The tokens are moved and the actions are executed the same as with usual transition clearings.
Tokens of all predecessor steps are removed and tokens of all successor steps are created. All P0 actions linked to predecessor steps and P1 - S - R - N actions linked to successor steps are executed.
This illustrates cycle execution when forcing transition clearing:
sfc5_tcf
IMPORTANT:
  • Clearing a transition may cause abnormal behavior of a chart since several tokens may be created.
  • Do not clear transitions located under parallel branches.
To clear a transition
  • Right-click the transition while in simulation mode, and then click
    Clear Transition
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal