Breakpoint on Transition
When a transition becomes clearable (transition is valid, for example all previous steps are active, and its receptivity is true) then breakpoint mode is set for the next cycle. The current cycle goes on executing normally except that the transition is not cleared and therefore related tokens are not moved.
This illustrates cycles execution when a breakpoint on transition is encountered.

To set a breakpoint on a transition
- Right-click the transition, and then clickSet Breakpoint.
Provide Feedback