OR_MASK
Integer OR bit-to-bit mask.

Arguments | |||
|---|---|---|---|
IN | IN | DINT | Must have integer format |
MSK | MSK | DINT | Must have integer format |
OR_MASK | Q | DINT | Bit-to-bit logical OR between IN and MSK |
Example
(* FBD example with OR_MASK Operators *)

(* ST Equivalence: *)
parity := OR_MASK (xvalue, 1); (* makes value always odd *) result := OR_MASK (16#abc, 16#f0f); (* equals 16#fbf *)
Provide Feedback