CTUD
Counts (integer) from 0 up to a given value 1 by 1 or from a given value down to 0 1 by 1

Arguments | ||
|---|---|---|
CU | BOOL | Up-counting (when CU is a rising edge) |
CD | BOOL | Down-counting (when CD is a rising edge) |
RESE | BOOL | Reset command (dominant) (CV = 0 when RESET is TRUE) |
LOAD | BOOL | Load command (CV = PV when LOAD is TRUE) |
PV | DINT | Programmed maximum value |
QU | BOOL | Overflow: TRUE when CV >= PV |
QD | BOOL | Underflow: TRUE when CV <= 0 |
CV | DINT | Counter result |
Example
(* FBD program using the CTUD block *)

(* ST Equivalence: We suppose CTUD1 is an instance of block*)
CTUD1(trigger1, trigger2, reset_cmd, load_cmd,100); full := CTUD1.QU; empty := CTUD1.QD; nb_elt := CTUD1.CV;
Provide Feedback