Vertical Bars
Vertical bars are graphic components of Functional Block Diagram (FBD) programs enables closing multiple parallel links. More than one horizontal links on the left side of a vertical bar are connected to one link on the right side. The Boolean state of the right end is the logical OR between all the left extremities.

To insert a vertical bar
- From theToolbox, drag the vertical bar element into the language container.The vertical bar appears in the language container.
Provide Feedback