FBD Diagram Main Format

Function Block Diagram (FBD) diagrams describe a process between input variables and output variables. A process is described as a set of elementary blocks. Input and output variables are connected to blocks by connection lines. Outputs of blocks can also be connected to inputs of other blocks.
fbd_mf1
An entire process represented by an FBD program is built using the available variables, operators, functions, and function blocks. Each block has either a fixed or defined number of input and output connection points. A block is represented by a single rectangle. The inputs are connected on its left border. The outputs are connected on its right border. An elementary block performs a single function between its inputs and its outputs. The name of the function to be performed by the block is written inside its rectangle shape. Each input or output of a block is labeled and has a well-defined type.
fbd_mf2
Input variables of an FBD program must be connected to input connection points of blocks. The type of each variable must be the same as the type expected for the associated input. An input for FBD diagram can be a literal, any internal or input variable, an output variable, or a block output.
Output variables of an FBD program must be connected to output connection points of blocks. The type of each variable must be the same as the type expected for the associated block output. An output for FBD diagram can be any internal or output variable, or the name of the function (for functions only). When an output is the name of the currently edited function, it represents the assignment of the return value for the function (returned to the calling program).
Input and output variables, inputs and outputs of the blocks are wired together with connection lines, or links. Single lines can be used to connect two logical points of a diagram:
  • An input variable and an input of a block
  • An output of a block and an input of another block
  • An output of a block and an output variable
The connection is oriented, meaning that the line carries associated data from left to right. The left and right ends of the connection line must be of the same data type.
Multiple right connections, also called divergences can be used to broadcast information from their left end to each of the right ends. All ends of the connections must be of the same data type.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal