Variables Grid
Use the variables grid of the
Dictionary
to manage the variables for a controller or program. Each controller and program has its instance of the grid. The grid displays global variables for controllers. The grid displays the local variables for programs. Perform these tasks from the variables grid:Task | Procedure |
|---|---|
Create a variable |
|
Edit an existing variable |
|
Drag a variable | Drag variables from a Dictionary instance to multiple locations within a project. These locations include other Dictionary instances and elements within a language container.Drag variables to other locations individually. When dragging a variable to another Dictionary instance, place the variable anywhere in the grid. When dragging a variable into a language container, place the variable anywhere in the language container. To retain changes made to Dictionary instances and language containers, save the respective instance or POU before closing.
|
Delete a variable | Deleting variables from an instance opened for a program element removes the variables from the instance only.
|
Cut, copy, and paste variables | When selecting variables, an indicator arrow ( ) displays in the leftmost column of the grid. Cut, copy, and paste variables from one Dictionary instance to another. Also cut, copy, and paste variables from the Variable Selector to the Dictionary.
|
Sort variables in the grid | Sort the variables in the grid using an ascending or descending order for the individual columns.
|
Filter variables in the grid | When filtering, create a view displaying only the variables containing specified characters. The filter row is the top row of the grid. Filter variables by typing alphabetical and numerical characters in the cells of the filter row. Also select from the drop-down combo box. Variables containing matching characters automatically display in the grid.
|
Add a variable to a variable group | In the variable grid, right-click the variable, point to Add to Variable Group , then click the required group. |
TIP:
Update each instance of a function or function block
after adding, removing, renaming, changing data type, or changing direction of parameters in
all POUs using the instance. Identify these POUs with the
Cross Reference Browser
,
then open each POU and reselect the modified instance using the Block
Selector
.For variables of controllers or programs, the properties are:
Column | Description | Possible Values |
|---|---|---|
Name | Name of the variable | Limited to 128 characters beginning with a letter or single underscore character followed by letters, digits, and single underscore characters. The last character for a variable name must be a letter or digit; variable names cannot end with an underscore character. Do not use reserved words, defined words, or data types (elementary, structures, or arrays) for names. Names must be unique for the same type of elements within a scope. |
Logical Value | Available when online. The display value depends on the direction of the variable. In the dictionary view, the columns display values for the variables used in controllers where debugging is enabled. | Input: Locked Output: Updated by the running TIC code Internal: Locked |
Physical Value | Available when online. The display value depends on the direction of the variable. In the dictionary view, the columns display values for the variables used in controllers where debugging is enabled. | Input: Updated by the field value Output: Locked Internal: Updated by the running TIC code |
Lock | Available when the application is connected. The value of the variable is locked. Enables locking only I/O variables. Locking operates differently for simple variables, array and structure elements, and function block parameters. For simple variables, individual variables are locked directly. For structure and array elements, locking an element locks only that element of the structure or array. | Yes or No |
Data Type | Data type of the variable. Avoid using library data types. | BOOL, BYTE, DATE, DINT, DWORD, INT, LINT, LREAL, LWORD, REAL, SINT, STRING, TIME, UDINT, UINT, ULINT, USINT, WORD, user arrays, and structures |
Dimension | Size (number of elements) of an array | For example: [1..3,1..10] - represents a two-dimensional array containing a total of 30 elements.
TIP:
Dimension does not apply to function
block instances. Avoid setting Dimension for function block instances to
help prevent unexpected build results. |
String Size | Maximum length for String-type variables | String capacity has a maximum of 255 characters excluding the terminating null character (0), a byte for the current length of the string, and a byte for the maximum length of the string. The default value is 80. |
Initial Value | Value held by a variable when the virtual machine starts the execution of the controller | The initial value of a variable. Possible values are the default value, a value assigned by the user when defining the variable, or the value of the retain variable after the virtual machine has stopped.
TIP:
Use a decimal value only. Hexadecimal
values are not supported.
|
Direction | For local variables of a program organization unit (POU), indicates whether the variable is internal, an input, or an output. | Possible values are Var, VarInput, or VarOutput. When wiring the local variable of a program, the direction changes to match the direction required by the I/O device. |
For global variables of a controller, indicates whether the variable is internal, an input, an output, or a system variable. | Possible values are Var, VarInput, VarOutput, VarGlobal, or VarDirectlyRepresented. When wiring a variable, the direction changes to match the direction required by the I/O device. | |
Attribute | Read and write access rights of a variable | Possible values are Read, Write, or Read/Write. The possible values depend on the direction of the variable. When wiring a variable, the attribute changes to match the direction required by the I/O device. |
Retained | The controller saves the value of the variable in non-volatile memory at each cycle. When setting the Retained property for a variable with a structure data type, the property is set for the entire structure; individual structure members cannot be retained.Limitations:
| True or False When the processor battery voltage is low or no battery is fitted, setting Retained to True has no effect. |
Comment | User-defined text | Plain text |
Alias | Any name (for use in POUs) | Limited to 128 characters consisting of letters, digits, and these special characters: !, #, $, %, &, \, *, +, -, /, <, :, =, >, ?, @, ^, _, `, |, and ~. |
Wiring | (Read-only) Generated by the I/O wiring tool indicating the I/O channel wired to the variable | Uses the syntax of directly represented variables |
Groups | Group name or "None" | |
Allow OPC Write | An external client can write to the variable. Only available for user-defined variables or user-defined instances of function blocks. | The default value is FALSE |
Message True | Message defined for the TRUE value message | Limited to 65535 characters |
Message False | Message defined for the FALSE value message | Limited to 65535 characters |
Customize the
Dictionary
environment by arranging the columns to display.Provide Feedback
) is displays in the leftmost column.