Defined Words Grid
Use the
Defined Words
grid of the Dictionary
to manage the defined words for a project. Perform these tasks from the defined words grid:Task | Procedure |
|---|---|
Create a defined word |
|
Edit an existing defined word |
|
Delete a defined word |
|
Sort defined words in the grid |
|
Filter defined words in the grid | Filter defined words in Defined Words grid. When filtering, create a view displaying only the defined words containing specified characters.The filter row is the top row of the grid. Filter defined words by typing alphabetical and numerical characters in the cells of the filter row. Also select from the drop-down combo box. Matching defined words are automatically displayed.
|
Properties for defined words are:
Property | Description | Possible Values |
|---|---|---|
Word | Name of the defined word | Limited to 128 characters beginning with a letter or single underscore followed by letters, digits, and single underscores. The last character for a defined word must be a letter or digit; defined words cannot end with an underscore character. Reserved words, defined words, or data types, such as elementary, structures, or arrays are not valid names. Use unique names for the same type of elements within a scope. |
Equivalent | String replacing the defined word during compilation. Example: the defined word "PI" is replaced by its equivalent "3.14159" | Limited to 128 characters |
Comment | Comment for the defined word | Plain text |
Customize the
Dictionary
environment by arranging the columns to display.Provide Feedback