Peer-to-Peer Digital Outputs
When configuring a digital output data block, define this property:
Property | Description |
|---|---|
Refresh Interval | The maximum number of milliseconds allowed between successive transmissions of the output data. Note that data is immediately sent following any change in the output state. Possible values range from 0 to 10000 ms. The default value is 2000 ms. Specify a value of 0 to send data during each application cycle. |
To configure a digital output data block
- In the Communication View, double-click the digital output data block.The Communication property page displays with theData BlockandData Variablestabs.
- In theData Blocktab, enter the required value for theRefresh Interval.
Provide Feedback