Peer-to-Peer Analog Outputs
When configuring an analog output data block, define these properties:
Property | Description |
|---|---|
Refresh Interval | The maximum number of milliseconds allowed between successive transmissions of the output data. Note that data is immediately sent following any change in the output state. Possible values range from 0 to 10000 ms. The default value is 2000 ms. Specify a value of 0 to send data during each application cycle. |
Minimum Change before Update | The minimum change in the value of the output variable required before an update is sent to the peer input, regardless of the Refresh Interval . Possible values range from 0 to 3.402823E+38. The default value is 0. When the data type of the output variable is DINT, the decimals are truncated. |
To configure an analog output data block
- In the Communication View, double-click the analog output data block.The Communication property page displays with theData BlockandData Variablestabs.
- In theData Blocktab, enter the required value for theRefresh IntervalandMinimum Change before Update.
Provide Feedback