AADvance Discover Features
Tasks to perform with AADvance Discover are:
Task | Procedure |
|---|---|
Configure the IP Address, Subnet Mask, Gateway, and Gateway Port in a controller |
|
Configure the Resource Number in a controller |
|
Configure Ethernet forwarding in a controller |
|
View the MAC Addresses of Ethernet ports |
|
Save the configuration of a controller |
|
Load the configuration into a controller |
|
Configure the IP Address of the controller in AADvance-Trusted SIS Workstation software |
|
Configure the resource number of the AADvance controller |
|
Using the
AADvance-Trusted SIS Workstation software
, configure the controller to use the same IP Address set in the physical controller.The AADvance controller provides up to six Ethernet communication ports, two for each 9110 processor module present. Each pair of Ethernet ports is identified as E
n
-1 and En
-2 where n indicates the processor module. The En
-1 Ethernet ports are all on one network and the En
-2 ports are on a second network.
TIP:
To avoid unexpected ARP requests, it is recommended to
configure IP addresses for E
n
-2 ports (even if they are unused).The AADvance controller stores the IP address data in non-volatile memory in the 9100 processor base unit. The controller retains the address information when removing a processor module since the data is independent of the 9110 modules.
Allocate a local network IP address or use an address from the following ranges of private networks:
- 10.0.0.0 to 10.255.255.255
- 172.16.0.0 to 172.31.255.255
- 192.168.0.0 to 192.168.255.255
Each controller on a local area network must have a unique IP address.
IMPORTANT:
The two Ethernet ports on each 9110 processor
module must be on different subnets.
Only define one Gateway address per processor module.
IMPORTANT:
Communication blocking or miss-routing by
Windows®
(or other network devices) can cause the AADvance Discover
tool to omit displaying certain controllers. DCP communications are unable to go through
network bridges and routers. When using virtual machines, use a direct bridged connection.
It may be necessary to disable firewalls blocking access to AADvDiscover.exe.AADvance Discover is accessible from the
Windows
Start menu or from the AADvance-Trusted SIS Workstation software
(in the View menu).The DCP is proprietary to
Rockwell Automation®
. The protocol uses the MAC address of the 9100 processor base unit to identify individual controllers. In AADvance Discover, the MAC address of the base unit displays as the Controller ID. Also view the MAC addresses of the six Ethernet ports.A controller has one of the following statuses:
Status | Description |
|---|---|
Configurable | The controller is available for configuration. The following criteria are satisfied:
Set the Resource Number , IP Address , Subnet Mask , Gateway , and Gateway Port information for this controller. |
Locked | AADvance Discover has established communications with the controller, but one or more of the following criteria is not satisfied:
Resource Number , IP Address , Subnet Mask , Gateway , and Gateway Port information for this controller are view only. |
No Response | The controller is turned off or the communications between the computer running AADvance Discover and the controller have failed. |
Pending Restart | Restart the controller after making modifications to a controller available for configuration. Before restarting the controller, modify the Resource Number , IP Address , Subnet Mask , Gateway , and Gateway Port information. |
Click Refresh in the AADvance Discover tool to update the list of controllers. When refreshing, a status bar displays at the bottom of the window, below the list. The status bar displays the following messages:
- Initializing, the AADvance Discover tool starts
- Searching, the tool locates all the controllers connected to the network
- Querying, the tool displays the resource number and status of the controllers
- Ready, the information that displays in AADvance Discover is ready for use
Provide Feedback