AADvance Discover

Use
AADvance Discover
to set the IP address for the physical controller. Configure the resource number and IP address when assembling a new AADvance controller or installing a new 9100 processor base unit. Also configure Ethernet forwarding if required. The
AADvance Discover
tool uses a discovery and configuration protocol (DCP) to scan the broadcast domain for AADvance controllers. The tool then displays a list of AADvance controllers and their statuses. Refresh the list of controllers.
TIP: Before using
AADvance Discover
, disable connections to networks other than the
AADvance® Control System
network.
advd_ad1
From AADvance Discover, access the
Controller Configuration
dialog box, enabling the configuration of the
Resource Number
,
IP Address
,
Subnet Mask
,
Gateway
, and
Gateway Port
values to be stored in a physical controller. For
Locked Controllers
, this information is view only. Also use the
Controller Configuration
dialog box to save and load controller configurations.
advd_ad2
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal