FM_WRITE
Writes message variables to a binary file. For use with F_WOPEN and F_CLOSE. A message is written in the file as a null terminated string. This procedure makes a sequential access to the file, from the previous position. The first call after F_WOPEN writes the first string to the file, each call pushes the writing pointer.
IMPORTANT:
Avoid using this function. This function is
intended to be obsolete.

Arguments | ||
|---|---|---|
ID | DINT | File number: returned by F_WOPEN |
IN | MESSAGE | Message value to be written in the file |
OK | BOOL | Execution status: TRUE if successful |
Example
(* FBD program using file management blocks *)

(* ST Equivalence: *)
file_id := F_WOPEN('trace.txt'); ok := FM_WRITE(file_id,'First message'); ok := FM_WRITE(file_id,'Last message'); ok := F_CLOSE(file_id);
Provide Feedback