DAY_TIME
Gives date or time of the day as a message string.

Arguments | ||
|---|---|---|
SEL | DINT | output selection 0= get current date 1= get current time 2= get day of week |
Q | MESSAGE | time/date expressed on a character string ''YYYY/MM/DD' if SEL = 0 ''HH:MM:SS' if SEL = 1 day name if SEL = 2 (ex: 'Monday') |
Example
(* FBD Program using "DAY_TIME" function *)

(* ST Equivalence: *)
Display := Day_Time (0) + ' ; ' + Day_Time (1); (* Display text format is: 'YYYY/MM/DD ; HH:MM:SS' *)
Provide Feedback