CAT
Concatenates 2 to 32 messages into one message.

Arguments | ||
|---|---|---|
(inputs) | MESSAGE | From 2 to 32 inputs. The output message capacity limits the length of the
concatenated message. |
output | MESSAGE | Concatenation of the input messages. |
Example
(* FBD example with "CAT" Operator *)

(* ST equivalence: *)
MyName := ('Mr' + ' ') + 'Jones'; (* means: MyName := 'Mr Jones' *)
Provide Feedback