Export a function block

Export function blocks as exchange files (*.txf) to import them into different projects. Importing exchange files enables reusing function blocks in different
Trusted®
projects. Export individual function blocks.
TIP: Exporting a program, function, or function block exports its logic, local variables, local defined words, and description. Program, function, and function block comments, Diary files, and Modbus® extended attributes are not exported.
To export a function block
  1. In the
    Application View
    , right-click the function block, and then click
    Export...
    .
  2. In the
    Save Function Block As
    dialog box, browse for the location to store the
    Trusted
    exchange file, and then click
    Save
    . The function block is exported as an exchange file.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal