Add a function block from an exchange file

Import function blocks previously exported as exchange files (*.txf). Importing exchange files enables reusing function blocks in different
Trusted®
projects.
TIP: Importing a program, function, or function block imports its logic, local variables, local defined words, and description. Program, function, and function block comments, Diary files, and Modbus® extended attributes are not imported.
When importing a program organization unit (POU), specify a unique name within the project.
To add a function block from an exchange file
  1. In the
    Application View
    , right-click
    Function Blocks
    , point to
    Add Function Blocks
    , and then click
    Existing Function Block...
    .
    TIP: Alternatively, add an existing program from
    File > Add > Existing Function Block...
  2. In the
    Select Exchange File
    dialog box, locate the
    Trusted
    exchange file containing the function block, and then click
    Open
    . The function block is imported into the project.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal