Securable Actions supported by FactoryTalk Security
FactoryTalk Security
Configure the securable actions listed here in the Network Directory by using the which is available in the Rockwell Automation Literature Library.
FactoryTalk Administration Console
. For details, see the FactoryTalk Security
System Configuration Guide
TIP:
The variable selector normally opens with a data type filter and an empty row
at the bottom of the grid. Selecting the empty row clears the filter. The securable actions
Project: Modify Global Variables, Project: Modify POUs, and Project: Modify Global Library
set to Deny might influence the variable selector behavior. Clear the filter to see the
variables in the variable selector. For instructions on how to reset the filter, see Variable Selector.
These are the
FactoryTalk Security
securable actions.Action | Description |
|---|---|
Application: Verify, Build or Clean | Verify a POU syntax, build an application, or clean an application. |
Controller: Connect | Connect to a controller. |
Controller: Download | Download an application. |
Controller: Lock/Unlock Variables | While connected, lock or unlock the value of a variable. |
Controller: Modify Cycle Timing | Edit the cycle timing. |
Controller: Open Intelligent Update Manager | Open the Intelligent Update Manager tool. |
Controller: Open System Configuration Tool | Open the System Configuration Tool. |
Controller: Override Variables | While connected, force the value of a variable. |
Controller: Spy Lists | Monitor a list of variables. |
Controller: Start/Stop | Start or stop an application. |
Controller: Update | Update an application. |
Project: Configure I/O Devices | Edit instances of I/O devices and edit the wiring of a channel. |
Project: Configure ISaVIEW | Edit an ISaView document. When ISaVIEW securable Action is set to Deny, ISaVIEW objects/shapes properties are not visible from the Property Window and the entire document is read-only. |
Project: Configure Password | Add, change, or remove a password on a project. |
Project: Configure Permission Set | Select, or remove a permission set associated with a project. |
Project: Configure POUs | Add, delete, rename, reorder, or import a POU in the device or in the global library. |
Project: Modify Communication Parameters | Modify communication properties. |
Project: Modify Compiler Options | Modify compiler options. |
Project: Modify Conversion Tables | Modify conversion tables. |
Project: Modify Description | Edit the project description. |
Project: Modify Global Defined Words | Edit global defined words. |
Project: Modify Global Library | Modify the global library. |
Project: Modify Global Variables | Edit or import global variables. |
Project: Modify POUs | Edit a POU in the device or in the global library, including: Local variables Local defined words Editors: Structured Text, Ladder Diagram, or Function Block Diagram. Diary Variables properties Import local variables |
Project: Modify Runtime Parameters | Modify application run-time options. |
Project: Modify SOE/Modbus Extended Attributes | Configure SOE or Modbus attributes for a global variable. |
Project: Open | Open the project. |
Project: Rename Device | Rename a target device. |
Provide Feedback