Preview Selections

Preview selections to modify objects and visualize the rotation, displacement, and size animation effects defined for selected individual and grouped objects. While previewing selections, objects and their properties can be modified; animation effects cannot be modified. However, since the size animation effect is defined as a percentage, the boundaries outlining this effect change as an object is resized.
Visualize the animation effects defined for selected individual and grouped objects from the colored indicators as follows:
isv_psl
The displacement for the
Animation
Position
property where the broken red line indicates the end position and path of travel for the object.
The rotation for the
Center
of
Rotation
property where the blue circle indicates the center of rotation for the object.
The size for the
Animation
Size
property where the green broken outline indicates the final size of the object.
Previewing screens is available while online.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal