Preview Animation Effects (Editable)

Graphically modify the rotation, displacement, and size properties for individual and grouped objects while in animation preview mode. Animation preview mode prohibits to add, delete, move, group, or ungroup objects. Graphically modify animation effects properties by repositioning the displayed indicators as follows:
isv_pan
  • The displacement indicator for the
    Animation
    Position
    property where the red dot and broken line indicate the end position and path of travel for the object.
  • The rotation indicator for the
    Center
    of
    Rotation
    property where the blue dot indicates the center of rotation for the object.
  • The size indicator for the
    Animation
    Size
    property green dot and broken lines indicate the final size of the object.
Previewing screens is available while online.
Access the animation preview mode from the
ISaVIEW
toolbar.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal