Edit the points of an existing conversion table
Edit the points of a conversion table to modify the proportional relationship between electrical values and physical values used in application programming.
To edit the points of an existing conversion table
- From theApplication View, right-click the device, and then clickConversion Tables.
- In theConversion Tablessection, select the conversion table to modify.
- In theDetailssection, modify the conversion table:
- To edit the values of existing points, enter the new value then press (RH: select)Enter.
- To add a conversion point, clickAdd, and then enter theElectricalandPhysicalvalues for the point.TIP: Each conversion table can have a maximum of 32 points.
- To remove conversion points, select the points and then clickRemove.A line graph representing the conversion table and its modifications displays on the right-hand side of theConversion TableEditor.
Provide Feedback