Create a conversion table
A conversion table is a set of points defining an analog conversion. Apply a conversion table to an analog input or output variable to create a proportional relationship between electrical values (read on input sensor or sent to the output device) and physical values used in application programming.
TIP:
Trusted®
projects can have a
maximum of 127 conversion tables.A conversion table filters the values of any input or output analog variable of a project. Attach a conversion table to a variable from the
I/O Wiring
.
IMPORTANT:
Create conversion tables from the device level
before attaching these to variables.
To apply a conversion table to analog variables
- From theApplication View, right-click the device, and then clickConversion Tables.TheConversion Tables Editorappears.
- In theConversion Tablessection, clickAdd.A conversion table is added to the list.
- In theDetailssection, specify a name for the conversion table, then define the required points for the conversion by clickingAdd.TIP: Each conversion table can have a maximum of 32 points.
- Set theElectricalandPhysicalvalues for each point. A line graph representing the conversion table appears on the right-hand side of theConversion Table Editor.
Provide Feedback