Cleaning a Trusted Project
Trusted
ProjectDelete intermediate and output files belonging to projects or devices. Cleaning projects, or deleting these files, enables the generation of new files during the next build operation. When cleaning the device, the intermediate and output files are deleted for the device only.
After cleaning a project or device, regular updates cannot be performed. To retain the capacity to perform regular updates, perform a subsequent build rather than cleaning and then building. intelligent updates may still be performed after cleaning a project or device.
Task | Procedure |
|---|---|
Clean a project | In the Application View , right-click the project to clean, and then click Clean All . |
Clean a device | In the Application View , right-click the device to clean, and then click Clean . |
Provide Feedback