Verifying POU Syntax

Choose to verify the syntax for programs, functions, and function blocks. Also verify the syntax of functions and function blocks belonging to a library. When verifying the syntax, the
AADvance-Trusted SIS Workstation software
only verifies the programming syntax without producing code. View the verification progress in the
Output
window.
To verify POU syntax
  1. In the
    Application View
    , right-click the program, function, or function block, and then click
    Verify <POU>
    .
  2. (optional) To view the verification progress and generated errors, from the
    Tools
    menu, click
    Options
    .
    1. In the
      Options
      dialog box, expand
      Projects
      , click
      General
      , select these options, and then click
      OK
      .
      • Always show Error List if build finishes with errors
      • Show Output window when build starts
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal