TOF
Increases an internal timer up to a given value.

Arguments | ||
|---|---|---|
IN | BOOL | When detecting a falling edge, starts increasing the internal timer. When detecting a rising edge, stops and resets the internal timer. |
PT | TIME | This input defines the maximum programmed time. |
Q | BOOL | If Q is TRUE = total time is not elapsed. |
ET | TIME | This output determines the current elapsed time. |
Timing diagram

Provide Feedback