STACKINT
Manages a stack of integer values.
The STACKINT function block includes a rising edge detection for both PUSH and POP commands.
The maximum size of the stack is 128. The application defined stack size N cannot be less than
1 or greater than 128.
The OFLO value is valid only after a reset (R1 has been set to TRUE at least once and back to
FALSE).
Arguments | ||
|---|---|---|
PUSH | BOOL | Push command (on rising edge only) add the IN value on the top of the stack |
POP | BOOL | Pop command (on rising edge only) delete in the stack the last value pushed (top of the stack) |
R1 | BOOL | Resets the stack to its empty state |
IN | DINT | Pushed value |
N | DINT | Application defined stack size |
EMPTY | BOOL | TRUE if the stack is empty |
OFLO | BOOL | Overflow: TRUE if the stack is full |
OUT | DINT | Value at the top of the stack |
Example
(* FBD program using the STACKINT block: error management *)

(* ST Equivalence: We suppose STACKINT1 is an instance of STACKINT block *)
STACKINT1(err_detect, acknowledge, manual_mode, err_code, max_err); appli_alarm := auto_mode AND NOT(STACKINT1.EMPTY); err_alarm := STACKINT1.OFLO; last_error := STACKINT1.OUT;
Provide Feedback