INTEGRAL
Integrates a real value.

Arguments | ||
|---|---|---|
RUN | BOOL | Determines the mode:
|
R1 | BOOL | Resets the override |
XIN | REAL | Uses any real value |
X0 | REAL | Defines the initial value |
CYCLE | TIME | The sampling period where the value ranges from 0ms to 23h59m59s999ms. If the CYCLE parameter value is less than the real duration of the cycle time in the virtual machine, the sampling period uses the real duration of the cycle time. |
Q | BOOL | (output) Determines if R1 reset the override: TRUE = R1 is FALSE FALSE = R1 is TRUE |
XOUT | REAL | (output) Results in the integrated output value |
Function Block Diagram

(* ST Equivalence: INTEGRAL1 instance of INTEGRAL block *)
INTEGRAL1(manual_mode, NOT(manual_mode), sensor_value, init_value, T#100ms); controlled_value := INTEGRAL1.XOUT;
Provide Feedback