Rungs
Rungs are graphic components of Function Block Diagram (FBD) programs and represent a group of circuit elements leading to the activation of a coil. Dragging the rung element into the workspace inserts a left power rail linked to a right power rail. Also, the rung contains a direct contact and a direct coil. Error symbols (
) indicate that the direct contact and direct coil are undefined.
) indicate that the direct contact and direct coil are undefined.
To insert an FBD rung
- From theToolbox, drag the rung element into the language container.
Provide Feedback