FBD Variables
To connect a new symbol to an existing one (another variable, a block
input, or a block output) in the workspace, keep the mouse button depressed (the cursor
becomes a "ghost" symbol) and drag the element until its connecting line on the left (or
right) overlaps an existing connecting point. When the mouse is released, the new symbol is
automatically created and linked.
- Drag to place the existing element:

- Release the mouse button. The variable is automatically connected:

Replace existing variables in program organization units (POUs) by double-clicking them
to access the Variable Selector or single-clicking them to select from a drop-down combo-box
containing the global and local variables. Also, single-click a variable, then type a
literal value in the text box provided. When inserting literal values beginning with a
letter or an underscore, enclose these in single quotes as follows: 'abc'
- Select a variable from the drop-down combo-box:

- Type a literal value in the text box:

When selecting items like local variables, global variables, and defined words from the
drop-down combo-box, typing characters in the text box focuses on the possible
items.
For input and output variables, choose to display comments entered in the
dictionary. From the
View
menu, access the Properties
window and define the
Comment Position
property.
Resize variables that display in the
workspace.
To insert a variable
- From theToolbox, drag the variable element into the language container. TheVariable Selectoris displayed.
- In theVariable Selector, select the required variable, then clickOK.
Provide Feedback