Set Coil
Set coils enable a Boolean output of a connection line Boolean state.
![]() | |
Left Connection | Right Connection |
The associated variable is set to TRUE when the Boolean state of the left connection becomes
TRUE. The output variable keeps this value until an inverse order is made by a RESET coil. The
state of the left connection is propagated into the right connection. The right connection can
be connected to the right vertical power rail.
Example

(* ST Equivalence: *)
IF input1 THEN output1 := TRUE; END_IF; IF input2 THEN output1 := FALSE; END_IF;
Provide Feedback