Coils
Coils are graphic components of Ladder Diagram (LD) programs used in Function Block Diagram
(FBD) programs representing the assignment of Boolean outputs. A coil represents an action.
It must be connected on the left to a Boolean symbol, like a contact or the Boolean output
of a block.
Types of coils available from the FBD toolbox are:
- Direct Coil
- Reverse Coil
- Set Coil
- Reset Coil
Change the type of a coil at anytime after insertion.
When inserting coils in program organization units (POUs), assign variables using the
Variable Selector
. Names of assigned variables display above the coil elements
within POUs. Replace existing variables by double-clicking the variable names to access the
Variable Selector
or by single-clicking variable names to select from drop-down
combo-boxes containing the global and local variables. Also, single-click existing
variables, then type literal values in the text boxes provided. When inserting literal
values beginning with a letter or an underscore, enclose the variable name in single quotes
as follows: 'abc'.- Select a variable from the drop-down combo box:

- Type a literal value in the text box:

Task | Procedure |
|---|---|
Insert an FBD coil |
|
Insert a parallel FBD coil |
|
Change the type of a coil in FBD |
|
Provide Feedback