Tree view for block cross references
The
References
pane displays additional information for the cross references of a block graphically from the Tree view.
Item | Name | Description |
|---|---|---|
![]() | Common path | The common path of the block selected in the Elements pane and the number of cross references. |
![]() | Program organization unit (POU) | The name of the POU using the block and the quantity of cross references. |
![]() | Called by | The defined word is used by the POU. |
![]() | Block | Name of the function, function block, or operator. |
![]() | Location | Location of the cross reference in the language editor grid. |
Provide Feedback