View cross references of a block
Update the
Cross Reference Browser
to display current cross references in the project.The
Blocks
view of the Cross Reference Browser
displays cross reference data for functions, function blocks, and operators. Property | Description |
|---|---|
Name | Name of the function, function block, or operator. |
Count | Total number of cross references for a block in the program organization units (POUs) of a project. Accepted values are 0 or more. |
Category | Type of function, function block, or operator. Accepted values are standard or user-defined. |
Language | Programming language of the function, function block, or operator. |
Alias | A user-defined name for use with Ladder Diagram program organization units (POUs). |
Project | Project using the block |
Device | The name of the device using the block |
Resource | The name of the device using the block |
Comment | Free-format text describing the block |
To view cross references of a block
- In theCross Reference Browser, select theBlocksview, and then click
Update Cross Reference Data.The cross references update. - In theElementspane, select the block. The cross references for the selected block appear in theReferencespane.TIP: From theElementspane, expand individual blocks to view the inputs and outputs. Select user-defined functions and function blocks to view the cross reference data for each parameter.
- Right-click the cross reference and clickGo to Reference. The language container displays the cross reference of the block.
Provide Feedback