Arc Settings
Use the arc settings to specify default values for the individual object properties.
To specify the default settings for arc objects
- From theToolsmenu, clickOptions.
- From theOptionsdialog box, expandISaVIEWSettings, then expandISaVIEWObjectSettings, and then clickArcSettings.
- Specify the default values for the required properties, then clickOK.
Provide Feedback