Quick Find
When all search options are defined, choose to find the next instances of the required string or expression within the specified scope.
- When usingFindandReplace, perform searches and replacements for a selected POU body.PressCTRL+F,set theLookInfield toCurrentDocumentand use only theFindNextorReplacecommands.FindandReplaceretains the last searched string for a specific document. Enter a different string in theFindwhatbox.Search optionDescriptionProcedureFind whatString or expression to find within the open document.Type the required string into the field, select one of the last twenty searches from theFindwhatdrop-down combo box, and use regular expressions in searches.Look inScope for the search.Select the required scope from theLookindrop-down combo box.Find optionsOptions to refine the search.Search for case sensitive matches usingMatchCase. Disregard partial word matches by selectingMatchwholeword. Include regular expressions by selectingUseRegularExpressions. Also define the file types to search in theLookatthesefiletypestext box.Result optionsOptions for search results.Choose to display the results in theFindresults1windoworFindresults2window. Choose to display only file names in the search results by selectingDisplayfilenamesonly.
Task | Procedure |
|---|---|
Find a string or expression in a file | Perform searches for a selected program organization unit (POU) body.
|
Use regular expressions when finding strings or expressions |
|
Provide Feedback