Find and Replace Utility
Use the
Find
and
Replace
to perform these operations:- QuickFind: Find strings or expressions in files using theQuickFindutility.QuickFindsteps from one search result to the next in sequence, either backwards or forwards from the insertion point. When reaching the end or beginning of a document,QuickFindautomatically jumps to unsearched sections. When the search is complete, a message displays.
- QuickReplace: Replace strings or expressions in files using theQuickReplaceutility. Quick Replace steps from one search result to the next in sequence, either backwards or forwards from the insertion point. When reaching the end or beginning of a document,QuickReplaceautomatically jumps to unsearched sections. When the search is complete, a message displays.
Provide Feedback