Parameters Display
The parameters display graphically presents the parameters for a program organization unit
(POU) selected in the
Block
Selector
. When selecting a POU from the block list, the parameters display
automatically shows the local, input, and output parameters. Expand all or collapse all
parameters for POUs.
To expand or collapse all input and output parameters
- In the block list, select the required block for which to display the existing parameters.
- To expand all parameters, right-click in the parameters display, then clickExpandAll.
To collapse all parameters, right-click in the parameters display, then click
Collapse
All
.Provide Feedback