Loading
Blog
Recent ActivityRecent Activity

Turn Issues into Advantages with Advanced Movement

Overcome key challenges by embracing advanced motion and robotics technology

Share This:

LinkedInLinkedIn
XX
FacebookFacebook
PrintPrint
EmailEmail
Engineer, manager, inspector, checking and analysis data controlling of automation robot arms machine in factory industrial on system of software welding robotics and digital manufacturing operation.

Introduction: Material Movement Is Now a Strategic Advantage

In today’s manufacturing landscape, material movement is no longer just a support function - it’s a performance lever. As production environments grow more dynamic, with increasing SKU variation, shorter customer lead times, and relentless pressure on cost and quality, inefficient material flow becomes a silent drain on operational performance.

But here’s the opportunity: the same challenges that strain traditional systems can become sources of competitive advantage when approached with advanced motion, robotics, and unified control technologies.

Modern material movement solutions are transforming how manufacturers think about flexibility, productivity, and resilience.

Challenge 1: Manual Material Handling - and how automation turns it into a strength

The problem:

Manual handling is still widespread across many industrial operations. Relying on people to move raw materials between processes, and finished goods off the line drains labor resources, introduces ergonomic and safety risks, and slows throughput—especially in high-mix production where variability is constant.

The solution:

Autonomous Mobile Robots (AMRs) elevate material handling from a manual task to an automated, intelligent workflow.

OTTO® AMRs create advantages by:

  • Navigating dynamically using AI‑driven path planning
  • Integrating with production schedules and line status
  • Reducing dependency on scarce labor
  • Improving uptime through predictable, repeatable material delivery

They free workers to focus on higher‑value tasks and help create a safer, more efficient production environment.

Challenge 2: Frequent Changeovers - and turning flexibility into speed

The problem:

Fixed conveyors and mechanically linked systems struggle with rapid, frequent changeovers. High‑mix, low‑volume production exposes the limitations of rigid mechanical setups that require manual adjustments and generate downtime.

The solution:

Independent Cart Technology (ICT) transforms changeovers into a digital process rather than a mechanical one.

With magnetically propelled, individually controlled carts, manufacturers can benefit from:

  • Rapid SKU transitions
  • Higher throughput in the same footprint
  • Highly precise motion control for complex applications
  • Reduced mechanical wear and maintenance

By removing the mechanical constraints, ICT enables flexibility at the speed of software.

Challenge 3: Disconnected Systems - and the power of Unified Robot Control

The problem:

Motion systems, robots, conveyors, safety controllers and vision systems often operate on separate platforms. This creates synchronization issues, extended commissioning times and difficulties scaling to more complex workflows.

The solution:

A unified robot control architecture brings robotics, motion, material transport, and safety together on one platform.

Benefits include:

  • Faster commissioning and reduced engineering hours
  • Better synchronization across devices
  • Simplified maintenance
  • End‑to‑end system visibility for more informed decision‑making

With every component speaking the same “language,” complexity drops—and performance rises.

Challenge 4: Space Constraints - and doing more in less space

The problem:

Manufacturers need compact, multifunctional systems to maximize floor space. Traditional setups often require separate machines for different tasks, increasing footprint and cost.

The solution:

Advanced motion and robotics enable multifunctional machines that combine operations like filling, cartoning, and palletizing in one footprint. Modular architectures allow manufacturers to deliver high-performance systems without excessive space requirements and enable:

  • Combining multiple operations in a single station
  • Optimizing floor space without sacrificing capability
  • Future‑proofing lines with scalable modules
  • Reducing total cost of ownership through shared components

Manufacturers can produce more—within the same or smaller footprint.

Challenge 5: Downtime and Inefficiency - and designing for success before you build

The problem:

Every minute of downtime matters. Manual changeovers, poorly coordinated workflows, and late‑stage surprises during commissioning create delays, cost overruns, and lost production.

The solution:

Digital design and simulation tools, such as Emulate3D™ software, allow material movement systems to be fully tested and adjusted in the digital world before being deployed in the physical world.

Manufacturers can:

  • Validate flows, capacity, and performance early
  • Identify bottlenecks before they appear on-site
  • Reduce commissioning time dramatically
  • Achieve smoother, faster go‑lives

Digital twins turn risk into predictability—and predictability into speed.

From challenge to competitive advantage: The real outcomes

When advanced material movement solutions are deployed holistically, the transformation is measurable:

  • Faster Time-to-Market: Virtual commissioning and modular architectures help reduce deployment time significantly.
  • Higher Throughput: Synchronized motion and robotics boost productivity and responsiveness.
  • Redeploy Workforce: AMRs and automated changeovers cut manual handling, allowing you to assign people to higher value tasks.
  • Enhanced Safety: Intelligent routing and integrated safety systems reduce risk.
  • Scalability: Modular platforms allow manufacturers to start small and expand as needs evolve.

A practical roadmap to get started

  • Assess current state: Identify bottlenecks in material flow and quantify their impact.
  • Define clear objectives: Whether your priority is flexibility, safety, or speed, align technology investments with strategic business outcomes.
  • Engage experts early: Work with trusted partner as Rockwell Automation, who can offer integrated platforms and proven application experience across motion, robotics, AMRs, safety and digital design.
  • Start small, scale fast: Begin with a pilot project using modular systems, then expand across lines and sites.
  • Use simulation to derisk decisions: Use simulation to validate designs and optimize performance before deployment.

Conclusion: Make the Smart Move

Material movement has become one of manufacturing’s most powerful levers for agility, efficiency, and competitiveness. By embracing advanced motion and robotics technologies, manufacturers can turn challenges into opportunity - and opportunity into advantage.

Ready to take the next step?

Talk to an expert

Published March 11, 2026

Topics: Optimize Production Advanced Motion & Robotics Motion Control

Ara Surenian
Ara Surenian
Production Logistics Business Manager, Rockwell Automation
Ara serves as the leader of the Production Logistics business unit at Rockwell Automation where he develops approaches to integrate advanced motion and robotics solutions to help customers automate and optimize end-to-end material movement for future-ready factories. Previously, he oversaw the company’s production planning and scheduling software portfolio. With four decades of experience in plant operations, lean manufacturing and digital transformation, Ara has consistently delivered significant enhancements across various manufacturing sectors.
Subscribe to Rockwell Automation

Receive the latest news, thought leadership and information directly to your inbox.

Subscribe now

You may also be interested in

Loading
Loading
Loading
Loading
  1. Chevron LeftChevron Left Rockwell Automation Home
  2. Chevron LeftChevron Left Com...
  3. Chevron LeftChevron Left News
  4. Chevron LeftChevron Left Blogs
  5. Chevron LeftChevron Left Turn Issues into Advantages with Advanced Movement